Featured Medical Application - Personal Activity Monitor
An activity monitor is a low-power, portable device used to measure and record such
things as body movement and temperature for the purpose of tracking physical performance and number of
calories consumed. Personal activity monitoring can provide an objective means for tracking
one's physical fitness progress.
An MCU should be chosen for its ability to handle the potentially substantial amount of
data from a 3-axis accelerometer. Battery efficiency is another consideration, which may or may not
present a trade-off with processor performance. When active, a 32-bit microcontroller
will typically consume more current; however, it may only need to remain in a non-sleep state for a fraction of
the time required by an 8-bit MCU.
Major subsystems include:
-
Microcontroller
-
Force and temperature sensing circuitry
-
I/O: keyboard and display or touchscreen
-
Connectivity: USB, Bluetooth etc.
-
Power management
Temperature
Battery
V
REF
AMP
RTC
User Input
Use with analog accelerometer
ADC
Fuel Gauge
MCU
V
REG
Bluetooth
PMIC
Display
USB
Personal Activity Monitor Block Diagram
View Product List
Accelerometers for Personal Activity Monitors
Accelerometers
are electromechanical devices used to measure acceleration, or rate of change in velocity over time, and are
used to sense vibration, shock, and orientation.
Accelerometer
types and technologies can vary depending on product size and application. Pedometers and activity monitors
that make use of accelerometers can achieve high accuracy and reliability.
Temperature Sensors for Personal Activity Monitors
A
temperature sensor
is a device that measures cold or heat as a temperature or temperature gradient. Many applications require
some implementation of temperature sensing and measurement. For
medical applications
a sensor with high resolution can be desirable, because the range of human body temperatures may span only a
very small part of the sensor's dynamic range.
Batteries for Personal Activity Monitors
Batteries
are a portable, wireless means of storing energy via the use of self-contained chemical cells. They can be
for one-time use and discarded, or recharged and reused. In essence, a
battery
is an energy storage device, but can only store and release electricity as direct current. Direct current is
a flat line at a given amplitude (until it declines as it is exhausted), versus alternating current, which
is a sinusoidal wave.
Voltage References for Personal Activity Monitors
A
voltage reference
produces a constant level of voltage over time regardless of load, changes in power supply, or temperature.
Voltage references are used in power supplies, analog-to-digital converters, digital-to-analog converters,
and many other applications where voltage levels must be maintained at a steady level. Without a
voltage reference
, precision is greatly affected and may render the device inoperable. Voltage references can vary greatly in
performance. A voltage reference for a power supply might hold its output to within only a few percentage
points off of its nominal or stated value; however, a voltage reference to instrumentation-level standards
are measured in parts per million regarding stability and precision to the nominal or specified value.
Amplifiers for Personal Activity Monitors
Amplifiers
have enormous voltage gain, use feedback to operate, and can be classified in different ways. They can be
identified by the device they are intended to drive (e.g., headphone amplifier, speaker amplifier), the
frequency range of the signal (e.g., RF, Audio), and by the function that they perform (e.g., low noise
amplifier, inverting amplifier, power amplifier.)
Battery Protection for Personal Activity Monitors
Battery protection circuits
are an electronic safeguard to prevent damage to internal electronics in the event of reverse battery
installation, accidental short circuiting, or other inappropriate operation. The simplest protection for
reverse
battery protection
is a diode in series with the battery, however protection circuit ICs offer more than just battery
protection and can increase the useful operating life of a rechargeable battery pack.
Real Time Clocks for Personal Activity Monitors
Real Time Clocks
(RTCs) are IC devices that keep track of time. A typical
RTC
can provide the time of day as well as the date via a serial bus such as I
2
C or SPI. Although similar in many ways, RTCs should not be confused with clock generators, which are used
to synchronize various parts of a circuit.
ADCs for Personal Activity Monitors
An
Analog-to-Digital Converter
(
ADC
or
A/D converter
) measures the magnitude of an input analog signal and converts it to a digital number that is proportional
to the magnitude of the voltage or current. An ADC often converts signals collected from the real-world to
digital signals for processing. One of the more important specifications of an ADC is the resolution that it
offers, which is the number of discrete values (represented in bits) that the
ADC
produces in relation to the analog signal it is converting. The more bits, the higher the resolution. A
higher resolution yields a more accurate approximation of the analog input.
Fuel Gauges for Personal Activity Monitors
A
battery fuel gauge
, or
state-of-charge
(
SOC
) indication, has evolved from a simple warning to a complex system level use of information, such as soft
shutdown to prevent data loss. Considerations that affect accurate accounting for remaining battery charge
include the effects of aging, self-discharge, and temperature variations. The value for full capacity is
obtained and algorithms are used to calculate the remaining capacity. The drawback of this approach is that
self-discharge is difficult to model since it is a function of aging and temperature.
MCUs for Personal Activity Monitors
The term "
MCU
" or "
processor
" refers to an electronic device that performs computational functions and carries out the instructions of a
stored program. Other terms for processor are
microprocessor
, central processing unit, and digital signal processor. Essentially, the processor refers to "the brains of
a computer."
Battery Chargers for Personal Activity Monitors
Battery charging
circuits are used to recharge batteries and are available in linear or switching topologies. They can be
completely autonomous in operation or used with a microcontroller. Generally speaking, integrated chip
charging technology can produce charge currents in a range from around 625 nA, to more than 4.5A.
Battery charger IC
s often do more than just charge; they can protect from overcharging, regulate voltage, and manage charging
from irregular sources such as energy harvesters or very low voltage sources. In portable technology,
battery chargers are indispensable.
Voltage Regulators for Personal Activity Monitors
DC/DC regulators
are circuits that convert DC voltage from one level to another and maintain that voltage to a constant
level.
Electronic systems often have several sub-circuits, each with its own voltage level requirement that may be
higher or lower than the main power supply.
Step-up converters
or
regulators
boost a
voltage
to a higher level. Step-down converters or regulators lower (or "buck") a voltage to a lower level. DC/DC
converters and controllers can also be used for the same purpose, but may offer options such as multiple
softstart levels, undervoltage lockout, protection against overvoltage and undervoltage, and programmable
short-circuit protection. All of these devices are considered to be in the same category of integrated
chips, typically categorized as power management devices."
Bluetooth for Personal Activity Monitors
Bluetooth
is the most widely supported technology standard for short-range wireless communication between multiple
devices. Bluetooth allows for simple, versatile wireless communication, and using a method of FHSS
(Frequency Hopping Spread Spectrum), is highly resistant to interference and inherently secure. With nominal
data rates of 3 Mb/s (Bluetooth 2.0) and 24 Mb/s (3.0+HS, 4.0),
Bluetooth
is suitable for exchanging small files and streaming audio.
USB Transceivers for Personal Activity Monitors
USB
is a standard connection interface between computers and digital devices. A USB transceiver is a physical
layer device that prepares data for transmission and then sends to, and receives data from, another
transceiver. The transceiver detects connection and provides the low level USB protocol and signaling. The
term "transceiver" indicates an implementation of both transmit and receive functions. It transmits and
receives, encodes and decodes data, provides error indication, implements buffers to stage data until it can
be managed, and adjusts for the clock rate from the serial stream on the
USB SuperSpeed
bus to match that of the "link layer" higher up on the communication stack.
Interface ESD for Personal Activity Monitors
Electrostatic Discharge
(
ESD
) is an instantaneous electric current that flows from a higher to a lower voltage potential without
warning. One of the more well-known causes of ESD is static electricity, which is created when insulator
surfaces rub together. Permanent damage can occur to semiconductor devices that are exposed to
ESD
. An ESD current waveform has an extremely fast rise time. ESD protection chips can be very effective but
consume board space and add capacitance to an I/O line.
Power Managment ICs for Personal Activity Monitors
A
Power Management Integrated Circuit
(
PMIC
) is a special-purpose IC that provides one or more power management related functions. These can include
voltage regulation, DC/DC conversion, battery management capability and more. Many PMICs offer an I
2
C and/or SPI bus interface, and some might provide additional features such as an integrated touch screen
interface.
Displays for Personal Activity Monitors
LCD
means "
liquid crystal display
." It is an electronically driven flat panel screen that orients liquid crystals within the panel in a
direction that blocks or transmits light coming from behind the panel. LCDs are a low cost, energy efficient
visual display that can be controlled in segments or as individual pixels, in shades of black and gray, or
in full color.
LCD
s have most commonly replaced bulky cathode ray tubes in televisions and computers and are available in all
sizes. Liquid crystals were first discovered in 1888, but were first put into common use in the early 1970s
as electronic digital-display watches.
USB Receptacles for Personal Activity Monitors
USB plugs and receptacles
are meant to reduce human error by their unique shape; they fit together in only one way. USB plugs and
receptacles come in Type A (typically connecting to hosts or hubs) or Type B (typically connecting to
devices) and 3 sizes: standard, mini, and micro. Type A plugs always face upstream, Type B faces downstream.
Wall Adapters for Personal Activity Monitors
An
AC/DC adapter
is a type of external power supply, often enclosed in what looks like an over-sized
AC wall-plug
. Other names include power adapter, power converter, plug-in adapter, adapter block, domestic mains
adapter, line power adapter, or simply AC adapter. AC adapters are used with electrical devices that require
DC power but do not have the internal circuitry to accomplish the conversion of AC to DC. Medical-grade
power supplies are designed to meet the IEC60601-1 medical equipment safety standard and may include typical
output voltages of 3.3 to 48 Vdc, a variety of package style (open-frame, enclosed, encapsulated, etc.),
mounting options, thermal management, and environmental features, among others.